This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EMIFA over PSP

Hi,

 

I use C6748 with PSP 01_30_01.  

I found that PSP includes EMIFA driver only for NAND flash.  

I use TFT display connected to EMIFA (motorola 68000like interface), so I need to configure the EMIFA in assynchronius  SRAM or SDRAM mode.

Is PSP provides such a driver or I need to build it in CSL level?

 

Thanks

Dani