Hi,
I mount m25p80 partition table under Linux, but not able to write the partition,
flash_eraseall: /dev/mtd3: Permission denied
what I could do to make it writable ?
trace: mtdchar.c found the mtd->flags must be MTD_WRITEABLE
and in board-da850-evm.c, I have made :
[2] = {
.name = "U-Boot",
.offset = MTDPART_OFS_APPEND,
.size = 288 * SZ_1K,
.mask_flags = MTD_WRITEABLE,
},
[3] = {
.name = "Logo Bmp",
.offset = MTDPART_OFS_APPEND,
.size = 160 * SZ_1K,
.mask_flags = MTD_WRITEABLE,
},
use mtd_debug info /dev/mtd3:
mtd.type = MTD_NORFLASH
mtd.flags = MTD_BIT_WRITEABLE
mtd.size = 153600 (150K)
mtd.erasesize = 4096 (4K)
mtd.writesize = 1
mtd.oobsize = 0
regions = 0
wired......
Best regards
Power Pan