I am using TCP2 in C6455. I don't know how to set the tail symbol registers (i.e. TCPIC6 to TCPIC11). The manual (pp. 50 to pp. 55 in SPRU973 May 2006) is not clear. It always talks about CDMA-2000. I have also looked at the code in the function TCP2_tailConfig3GPP(). I have tried using this code. The first canned Matlab testvector passes (i.e. TCP2 output bits match with Matlab generated bits). However the second test vector fails. I always use 161 as frame length. I am using TCP2 for 3GPP HSDPA decoding.