This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3517 Layout NAND Flash



Hi all,

does anybody know some links about Layout Guidlines of NAND Flash Memories?
Do I have to pay attention on length mismatch or impedance control (50 Ohm)?

Thanks!

Konrad


 

  • Hi Konard,

     

    According to me - You don't need to pay much attention for NAND Flash signal routing as , it is not high speed interface. It is better if you can match 50 Ohm impedance but if it is not possible then you can route those signal with 5 or 6 mil trace - or whatever you are using in your design.  Regarding Length I would say if  Nand data and control signals are matched with +/-20% tolerance it is fine. In my design I used to route this signal with 50 OHM and doesn't bother about length match as most of the time it is in +/-20% tolerance.

     

    Thanks,

    Rizwan Hirani