Dear All:
Our DM355 platform encounters a wired problem in the RX of the UARTs.
After DM355 runs for 2 weeks, the RX's of UART0 and UART1 are not working.
The same problem is reproduced after 3-4 hours of running DM355 inside the chamber in 50 degree C.
The CPU is still working by responding to the GPIO keys.
TX's seems OK. They continue to send out debug messages.
Is there any possible explanation to this problem?
Or, any one have the same experience?
Any comment will be welcomed.
best regards,
Ray