As title, when using the GenCodecPkg wizard in CCS 4.2.3 it does not find the algorithm properly. Here's what I do.
1. Create algorithm using GenAlg with default settings except for the format which is set to C674x ELF.
2. Import created CCS project into CCS and build it.
3. Close the built project.
4. Run GenCodecPkg and select the .genalg file created by GenAlg.
5. Fail.
At the last step the wizard does not let me continue onto the next screen as apparently it can't find the algorithm built in step 2.
Here is a screenshot where the wizard stops behaving:
Can someone help?
Thanks,
Ralph
P.S.
Here is a pic of my installed tools: