Other Parts Discussed in Thread: OMAP3530, FLASHTOOL
Hello, I am having the same problem as Simplesoft. Here was his post: "Good day! I build image of Windows Embedded Compact 7 for omap3530, but i have a problem when i boot image i've got message: and than system hold up and nothing happends. Somebody has solved a problem? Anybody can help me?" --------------------------------------------------------------------------------------------------------------------------------- I saw that the answer was to flash the files into memory, but I'm getting an error when flashing the NK.bin file. "¯ Operation FAILED (Remote: : size modulus 4 must be 0)" What settings should I use for the OMAP3530? Thanks!
-----------------------------------------------------------
[0]: Address=0x84001000 Length=0x02e3350c Save=0x80001000
-----------------------------------------------------------
Download file type: 1
rom_offset=0x0.
ImageStart = 0x84001000, ImageLength = 0x2e3350c, LaunchAddr = 0x8400cce0
Completed file(s):
-------------------------------------------------------------------------------
[0]: Address=0x84001000 Length=0x2e3350c Name="" Target=RAM
ROMHDR at Address 84001044h
Launch Windows CE image by jumping to 0x8000cce0...
Windows CE Kernel for ARM (Thumb Enabled)
--- High Performance Frequecy is 32768 khz---