Hi --
I have kind of an odd question. I am wondering if there is ECC protection on the L1 or L2 cache on the C6474?
Thanks,
Heather
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi --
I have kind of an odd question. I am wondering if there is ECC protection on the L1 or L2 cache on the C6474?
Thanks,
Heather
Heather Quinn said:I am wondering if there is ECC protection on the L1 or L2 cache on the C6474?
Someone else can confirm this but I don't believe any of the TI DSPs so far have had ECC protection on internal memories, generally they have been reliable enough to not need ECC by my understanding. I am kind of curious why you would be interested in this, are you working on a safety critical or hostile environment application?
OK, good to know.
My customer will be using them in a neutron-rich radiation environment, so, yes, it's a hostile environment. :-/
auppu35501 said:The C6474 does have ECC embedded in L2 cache and it also has Parity checking in L1P.
Thanks for the correction, I did not realize ECC was in there as I saw no mention of it in the datasheet, do you know if it is on any of the other C64x+ based devices or is this something that was added to C6474?
Hi Bernie,
The C6416 only had L2 parity check back then.
I think the first device to have ECC in L2 was C6455.
So, the list of devices which have L2 ECC and L1P Parity are:
C6455
C6457
C6474
C6472
For some reason its not mentioned in the datasheet.
Regards,
Arun