Other Parts Discussed in Thread: TMS320C6412
I am developping the communicataion card and i utilized tms320c6412 as cpci controller.
The card has to be installed in a chassis which has several slots and main controller(dual core, windows XP).
my question is
1. the system(chassis) do not recognize the card on some slots.
note : we can check the recognization of card through windows device manager
when recognization fail --> pci bridge property : "Code 12: This device cannot find enough free resources that it can use"
2. System recognize my card well if other commercial cpci card installed in other slot.
I will appreciate your reply ahead.