This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL138 debug

Hi,

I use dsplink_linux_1_65_00_03 in Linux. It works well.I hope I can use CCS 3.3 to debug the DSP program.As I know,CCS 3.3 and XDS560 JTAG EMULATOR don't support Linux system. So,can I develop ARM program with DSPLINK in Linux,and DSP program with DSPLINK in Windows? And  do DSPLINK has problem between the two programs?If not,how to debug the DSP program in Linux.

Thanks,

Yu