Hi Guys,
I'm trying to upload the demo randisk which is 12.6MB.
(http://arago-project.org/files/releases/davinci-psp_3.x.0.0-r37/images/dm6467t-evm/arago-demo-image-dm6467t-evm.ext2.gz)
When I start the transfer in the uboot enviroment using the 'tftp' command, the file starts loading after its quite a way through it hangs and I have to restart the board to get any response from it.
Transfering a file <9MB is file, is there a setting in uboot I need to change of is there something else that needs setting?
Thanks