This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NMI interrupt

Hello,

I am using omapL137 EVM starter kit, and I wrote a program on DSP part using DSP/BIOS.

I have a problem that my program suddenly jumps to another location from the same location in code each time. (more precisely it jumps after exit from one function to the start of another task)

I've changed the .text section location from SDRAM to IRAM (with same stack size) and it now jumps to NMI interrupt handler from the beginning. I am not sure that NMI location is coincidence.

What can cause this?

 

Thanks

Arye

  • Hi Arye,

    Your program could have a broken pointer, may be missing a crucial initialization, an exception may have occurred, etc..

    If it is a NMI exception occurrence, please look at the document (see page 53 ):

    TMS320C674x DSP CPU and Instruction Set User's Guide

     

  • Hi,

    Thank You for reply,

    I think I've located the problem - the software didnt crashed, it only jumped to interrupt vector, where the function was not defined for it.

    It happed because I've used the Event combiner uncorrectly.

    Can You maybe verify if the way I've used the combiner is correct? ->

    I am using OMAPL137:

    1. I've defined the combiner interrupts 0,1,2,3 to be on CPU interrupt vectors(4-15) vectors 7,8,9,10 respectively. In function handle for those interrupt I've put: ECM_dispatch.

    2. Enabled CPU interrupts 7,8,9,10.

    3. Since I am using the ECM for EDMA3, I've enabled the ECM module, and defined Events 8, 56,57,58:

                  a. handle to function to be executed for corresponding event.

                  b. Unmasked the event.

    Do I have to do anything else in order to enable interrupts through ECM module?

     

    Regards

    Arye Lerner.

     

  • Please look at pages 153/154 of the TMS320C6000 DSP/BIOS 5.32 Application Programming Interface (API) Reference Guide for all the steps you need. It seems you are correct.

    Have you enabled the ECM?

     

     

  • Hi,

    Yes I did, otherwise it generates an error. I am using LLD driver.

    I did everything as described in the document. When I use interrupt selector it works, when I switch to Event combiner it does not.

    I havent done any changes to driver's functions, exept of making some of the variables global (so I could complete the sequnce outside the function in interrupt generated on completion, instead of waiting in the loop inside function).

    In driver example, in init function this is used:

        ECM_dispatchPlug (ccXferCompInt, (ECM_Fxn)(&lisrEdma3ComplHandler0),&ecmattrs);
        ECM_enableEvent(ccXferCompInt);

    And lisrEdma3ComplHandler0 is a function I cannot find in *.C or *.H files in code. So I guessed that this function must be replaced by myEvent function, that I wrote to handle the event. But it didnt worked.

    Do I need to use ECM_dispatchPlug() at all, or when I configure the ECM module in DSP-BIOS confuguration tool this performed automatically?

    Regards

    Arye

  •  

    Arye Lerner said:

    In driver example, in init function this is used:

        ECM_dispatchPlug (ccXferCompInt, (ECM_Fxn)(&lisrEdma3ComplHandler0),&ecmattrs);
        ECM_enableEvent(ccXferCompInt);

    Can you point me to the file that contains that? I could not find it.

    Anyway, I would suggest you make a simple test case using ECM just to get familiar with it, and make it work. I would not start by editing the EDMA3 source code... 

     

    Arye Lerner said:
    Do I need to use ECM_dispatchPlug() at all, or when I configure the ECM module in DSP-BIOS configuration tool this performed automatically?

     You should not need that if you have done it statically.

    The only thing that I can think of is the Use Dispatcher and Argument in the HWI properties: 

     

     

    I looked at the example:

    C:\Program Files\Texas Instruments\pspdrivers_01_30_00_05\packages\ti\pspiom\examples\evm6747\i2c\interrupt\build\i2cSample.pjt

     The ECM co figuration itself is done by the driver, but the HWI config is made in the app. I looked at the HWIs, and it seems that not only the "Use Dispatcher" has to be checked, but the argument selected seems to match the "interrupt selection number" (in the case above = 1, events from 32 to 63), can you try putting the argument?

    Other than that I can not think about anything else...

     

  • /*
     * bios_edma3_drv_sample_init.c
     *
     * Sample Initialization for the EDMA3 Driver (for single-DSP based devices) for
     * BIOS 5 based applications. It should be MANDATORILY done once before EDMA3
     * usage.
     *
     * Copyright (C) 2009 Texas Instruments Incorporated - http://www.ti.com/
     *
     *
     *  Redistribution and use in source and binary forms, with or without
     *  modification, are permitted provided that the following conditions
     *  are met:
     *
     *    Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     *    Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the
     *    distribution.
     *
     *    Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
     *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
     *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
     *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
     *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
     *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
     *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
     *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
     *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
     *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
     *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     *
    */
    
    #include <ecm.h>
    #include <hwi.h>
    
    #include <ti/sdo/edma3/drv/sample/bios_edma3_drv_sample.h>
    
    
    /** @brief To enable the HWI event corresponding to the EDMA3
     * transfer completion ECM event.
     */
    #define EDMA3_HWI_BITMASK_XFER_COMP			(1u << hwIntXferComp)
    
    /** @brief To enable the HWI event corresponding to the EDMA3
     * channel controller error ECM event.
     */
    #define EDMA3_HWI_BITMASK_CC_ERR			(1u << hwIntCcErr)
    
    /** @brief To enable the HWI event corresponding to the EDMA3
     * transfer controller error ECM event.
     */
    #define EDMA3_HWI_BITMASK_TC_ERR			(1u << hwIntTcErr)
    
    /** @brief EDMA3 Driver Handle, used to call all the Driver APIs */
    EDMA3_DRV_Handle hEdma = NULL;
    
    /** @brief EDMA3 Driver Instance specific Semaphore handle */
    EDMA3_OS_Sem_Handle semHandle = NULL;
    
    
    /**
      * EDMA3 TC ISRs which need to be registered with the underlying OS by the user
      * (Not all TC error ISRs need to be registered, register only for the
      * available Transfer Controllers).
      */
    void (*ptrEdma3TcIsrHandler[EDMA3_MAX_TC])(unsigned int arg) =
                                                    {
                                                    &lisrEdma3TC0ErrHandler0,
                                                    &lisrEdma3TC1ErrHandler0,
                                                    &lisrEdma3TC2ErrHandler0,
                                                    &lisrEdma3TC3ErrHandler0,
                                                    &lisrEdma3TC4ErrHandler0,
                                                    &lisrEdma3TC5ErrHandler0,
                                                    &lisrEdma3TC6ErrHandler0,
                                                    &lisrEdma3TC7ErrHandler0,
                                                    };
    
    
    /**  To Register the ISRs with the underlying OS, if required. */
    void registerEdma3Interrupts (void);
    /**  To Unregister the ISRs with the underlying OS, if previously registered. */
    void unregisterEdma3Interrupts (void);
    
    /*
     *  ======== C64_enableIER ========
     *  enable interrupts specified by mask
     */
    extern Void C64_enableIER( Uns mask );
    
    
    /* External Global Configuration Structure */
    extern EDMA3_DRV_GblConfigParams sampleEdma3GblCfgParams;
    
    /* External Instance Specific Configuration Structure */
    extern EDMA3_DRV_InstanceInitConfig sampleInstInitConfig;
    
    /**
     * \brief SoC specific TC related information. Specified in the sample
     * configuration file (bios_edma3_sample_cfg.c).
     */
    extern unsigned int numEdma3Tc;
    extern unsigned int ccXferCompInt;
    extern unsigned int ccErrorInt;
    extern unsigned int tcErrorInt[8];
    extern unsigned int hwIntXferComp;
    extern unsigned int hwIntCcErr;
    extern unsigned int hwIntTcErr;
    
    /**
     * \brief   EDMA3 Initialization
     *
     * This function initializes the EDMA3 Driver and registers the
     * interrupt handlers.
     *
      * \return  EDMA3_DRV_SOK if success, else error code
     */
     EDMA3_DRV_Result edma3init ()
        {
        unsigned int edma3InstanceId = 0u;
        EDMA3_DRV_InitConfig initCfg;
        EDMA3_DRV_Result    edma3Result = EDMA3_DRV_SOK;
        EDMA3_OS_SemAttrs semAttrs = {EDMA3_OS_SEMTYPE_FIFO, NULL};
        EDMA3_DRV_GblConfigParams *globalConfig = &sampleEdma3GblCfgParams;
        EDMA3_DRV_InstanceInitConfig *instanceConfig = &sampleInstInitConfig;
        EDMA3_RM_MiscParam miscParam;
    
        if (NULL == hEdma)
            {
            /* configuration structure for the Driver */
            initCfg.isMaster    =    TRUE;
            initCfg.regionId = (EDMA3_RM_RegionId)1u;
            initCfg.drvSemHandle = NULL;
            /* Driver instance specific config NULL */
            initCfg.drvInstInitConfig = instanceConfig;
            initCfg.gblerrCb = NULL;
            initCfg.gblerrData = NULL;
    
            miscParam.isSlave = FALSE;
    
            /* Create EDMA3 Driver Object first. */
            edma3Result = EDMA3_DRV_create (edma3InstanceId, globalConfig ,
            									(void *)&miscParam);
    
            if (edma3Result != EDMA3_DRV_SOK)
                {
    #ifdef EDMA3_DRV_DEBUG
                EDMA3_DRV_PRINTF("edma3init: EDMA3_DRV_create FAILED\r\n");
    #endif
                }
            else
                {
                /**
                  * Driver Object created successfully.
                  * Create a semaphore now for driver instance.
                  */
                edma3Result = edma3OsSemCreate(1, &semAttrs, &initCfg.drvSemHandle);
                if (edma3Result != EDMA3_DRV_SOK)
                    {
    #ifdef EDMA3_DRV_DEBUG
                    EDMA3_DRV_PRINTF("edma3init: edma3OsSemCreate FAILED\r\n");
    #endif
                    }
                else
                    {
                    /* Save the semaphore handle for future use */
                    semHandle = initCfg.drvSemHandle;
    
                    /* Open the Driver Instance */
                    hEdma = EDMA3_DRV_open (edma3InstanceId, (void *) &initCfg,
                                            &edma3Result);
                    if(NULL == hEdma)
                        {
    #ifdef EDMA3_DRV_DEBUG
                        EDMA3_DRV_PRINTF("edma3init: EDMA3_DRV_open FAILED\r\n");
    #endif
                        }
                    else
                        {
                        /**
                         * Register Interrupt Handlers for various interrupts
                         * like transfer completion interrupt, CC error
                         * interrupt, TC error interrupts etc, if required.
                         */
                        registerEdma3Interrupts();
                        }
                    }
                }
            }
        else
            {
            /* EDMA3 Driver already initialized, no need to do that again. */
    #ifdef EDMA3_DRV_DEBUG
            EDMA3_DRV_PRINTF("edma3init: EDMA3 Driver Already Initialized...Init failed\r\n");
    #endif
            edma3Result = EDMA3_DRV_E_INVALID_STATE;
            }
    
         return edma3Result;
        }
    
    
    /**  To Register the ISRs with the underlying OS, if required. */
    void registerEdma3Interrupts (void)
        {
        unsigned int intState;
        ECM_Attrs ecmattrs = ECM_ATTRS;
        unsigned int numTc = 0;
    
        /* Disabling the global interrupts */
        intState = HWI_disable();
    
        /* Enable the Xfer Completion Event Interrupt */
        ecmattrs.unmask = 1u;
    	ecmattrs.arg = (Arg)0u;
    
        ECM_dispatchPlug (ccXferCompInt, (ECM_Fxn)(&lisrEdma3ComplHandler0),
                            &ecmattrs);
        ECM_enableEvent(ccXferCompInt);
    
        /* Enable the CC Error Event Interrupt */
        ecmattrs.unmask = 1u;
    	ecmattrs.arg = (Arg)0u;
    
        ECM_dispatchPlug(ccErrorInt, (ECM_Fxn)(&lisrEdma3CCErrHandler0), &ecmattrs);
        ECM_enableEvent(ccErrorInt);
    
        /* Enable the TC Error Event Interrupt, according to the number of TCs. */
        while (numTc < numEdma3Tc)
        {
            ecmattrs.unmask = 1u;
    		ecmattrs.arg = (Arg)0u;
    
            ECM_dispatchPlug (tcErrorInt[numTc],
                                (ECM_Fxn)(ptrEdma3TcIsrHandler[numTc]),
                                &ecmattrs);
            ECM_enableEvent(tcErrorInt[numTc]);
            numTc++;
        }
    
    
       /**
        * Enabling the HWI_ID.
        * EDMA3 interrupts (transfer completion, CC error etc.)
        * correspond to different ECM events (SoC specific). These ECM events come
        * under ECM block XXX (handling those specific ECM events). Normally, block
        * 0 handles events 4-31 (events 0-3 are reserved), block 1 handles events
        * 32-63 and so on. This ECM block XXX (or interrupt selection number XXX)
        * is mapped to a specific HWI_INT YYY in the tcf file. So to enable this
        * mapped HWI_INT YYY, one should use the corresponding bitmask in the
        * API C64_enableIER(), in which the YYY bit is SET.
        */
        /* To enable EDMA3 transfer completion interrupt */
    	C64_enableIER(EDMA3_HWI_BITMASK_XFER_COMP);
    	/* To enable EDMA3 CC Error interrupt */
    	C64_enableIER(EDMA3_HWI_BITMASK_CC_ERR);
    	/* To enable EDMA3 TC Error interrupt */
        C64_enableIER(EDMA3_HWI_BITMASK_TC_ERR);
    
        /* Restore interrupts */
        HWI_restore(intState);
        }
    
    
    /**
     * \brief   EDMA3 De-initialization
     *
     * This function removes the EDMA3 Driver instance and unregisters the
     * interrupt handlers.
     *
      * \return  EDMA3_DRV_SOK if success, else error code
     */
     EDMA3_DRV_Result edma3deinit (void)
        {
        unsigned int edmaInstanceId = 0;
        EDMA3_DRV_Result    edma3Result = EDMA3_DRV_SOK;
    
        /* Unregister Interrupt Handlers first */
        unregisterEdma3Interrupts();
    
        /* Delete the semaphore */
        edma3Result = edma3OsSemDelete(semHandle);
        if (EDMA3_DRV_SOK != edma3Result )
            {
    #ifdef EDMA3_DRV_DEBUG
            EDMA3_DRV_PRINTF("edma3deinit: edma3OsSemDelete FAILED\r\n");
    #endif
            }
        else
            {
            /* Make the semaphore handle as NULL. */
            semHandle = NULL;
    
            /* Now, close the EDMA3 Driver Instance */
            edma3Result = EDMA3_DRV_close (hEdma, NULL);
            if (EDMA3_DRV_SOK != edma3Result )
                {
    #ifdef EDMA3_DRV_DEBUG
                EDMA3_DRV_PRINTF("edma3deinit: EDMA3_DRV_close FAILED\r\n");
    #endif
                }
            else
                {
                /* Make the Drv handle as NULL. */
                hEdma = NULL;
    
                /* Now, delete the EDMA3 Driver Object */
                edma3Result = EDMA3_DRV_delete (edmaInstanceId, NULL);
                if (EDMA3_DRV_SOK != edma3Result )
                    {
    #ifdef EDMA3_DRV_DEBUG
                    EDMA3_DRV_PRINTF("edma3deinit: EDMA3_DRV_delete FAILED\r\n");
    #endif
                    }
                else
                    {
    #ifdef EDMA3_DRV_DEBUG
                    EDMA3_DRV_PRINTF("edma3deinit: EDMA3 Deinitialization" \
                                        " Completed...\r\n");
    #endif
                    }
                }
            }
    
        return edma3Result;
        }
    
    
    /**  To Unregister the ISRs with the underlying OS, if previously registered. */
    void unregisterEdma3Interrupts (void)
        {
        unsigned int intState;
        unsigned int numTc = 0;
    
        /* Disabling the global interrupts */
        intState = HWI_disable();
    
        /* Disable the Xfer Completion Event Interrupt */
        ECM_disableEvent(ccXferCompInt);
    
        /* Disable the CC Error Event Interrupt */
        ECM_disableEvent(ccErrorInt);
    
        /* Enable the TC Error Event Interrupt, according to the number of TCs. */
        while (numTc < numEdma3Tc)
        {
            ECM_disableEvent(tcErrorInt[numTc]);
            numTc++;
        }
    
        /* Restore interrupts */
        HWI_restore(intState);
        }
    
    /* End of File */
    
    Hi,

    Thanks for the patience,

    I also have this exact configuration.

    I used an example from:

    C:\Program Files\Texas Instruments\edma3_lld_01_10_00_01\packages\ti\sdo\edma3\drv\sample\src in file bios_edma3_drv_sample_init.c, function edma3init().

    I've copied all the required files to my project library. In addition to this I also enabled all four ECM interrupts (7,8,9,10) in HWI (by C64_enableIER())

    I've also attached this file, in case You dont have it (it is in txt, just change it to .c, if it matters).

    Can this example be used, or it is recommended to use the PSP?

    Thank You very much

    Arye