I'm seeing what appears to be an OMAP-3530 pin (specifically mcspi1_simo) that is configured as an output GPIO (PINMUX value 0x0204) and is outputting a low value unexpectedly shift to high-Z. I have observed this in two cases:
1. In OFF mode, and in both the case with off-output-low enabled and with off-mode disabled it goes high-Z.
2. With OFF mode enabled (/debug/pm_debug/enable_off_mode set to 1) and the pin outputting a 0, it periodically switches to high-Z for about 4ms every 5 seconds.
Any suggestions as to why this might be happening?
Thanks,
Chris