kiran@kiran-laptop:/opt/DM355SDK840402$ make Ridgerun Linux SDK Board configuration: Leopard Board Processing toolchain... Build complete Processing kernel... <stdin>:1097:2: warning: #warning syscall fadvise64 not implemented <stdin>:1265:2: warning: #warning syscall migrate_pages not implemented <stdin>:1321:2: warning: #warning syscall pselect6 not implemented <stdin>:1325:2: warning: #warning syscall ppoll not implemented <stdin>:1365:2: warning: #warning syscall epoll_pwait not implemented Kernel: arch/arm/boot/Image is ready Kernel: arch/arm/boot/zImage is ready Build complete Processing fs... Checking for host packages required by the SDK target applications... Host machine has all required packages. Entering host-apps... Entering apps... Checking dependencies for alsa-lib-1.0.21 Compiling and installing alsa-lib-1.0.21... Checking dependencies for alsa-utils-1.0.21 Checking dependencies for ncurses-5.6 Compiling and installing ncurses-5.6... Compiling and installing alsa-utils-1.0.21... Checking dependencies for busybox-1.14.2 Compiling and installing busybox-1.14.2... Checking dependencies for freetype-2.3.1 Compiling and installing freetype-2.3.1... Checking dependencies for gettext-0.16 Compiling and installing gettext-0.16... Checking dependencies for glib-2.16.5 Checking dependencies for libiconv-1.11 Compiling and installing libiconv-1.11... Compiling and installing glib-2.16.5... Checking dependencies for gst-plugins-bad-0.10.13 Checking dependencies for gstreamer-0.10.23 Checking dependencies for zlib-1.2.3 Compiling and installing zlib-1.2.3... Checking dependencies for libxml2-2.6.27 Compiling and installing libxml2-2.6.27... Compiling and installing gstreamer-0.10.23... Checking dependencies for liboil-0.3.15 Compiling and installing liboil-0.3.15... Checking dependencies for gst-plugins-base-0.10.23 Checking dependencies for libogg-1.1.3 Compiling and installing libogg-1.1.3... Checking dependencies for libvorbis-1.1.2 Compiling and installing libvorbis-1.1.2... Compiling and installing gst-plugins-base-0.10.23... Compiling and installing gst-plugins-bad-0.10.13... Checking dependencies for gst-plugins-good-0.10.14 Compiling and installing gst-plugins-good-0.10.14... Checking dependencies for gst-plugins-ugly-0.10.11 Compiling and installing gst-plugins-ugly-0.10.11... Checking dependencies for jpeg-6b Compiling and installing jpeg-6b... Checking dependencies for libpng-1.2.8 Compiling and installing libpng-1.2.8... Checking dependencies for mtdutils-1.0.0 Compiling and installing mtdutils-1.0.0... Checking dependencies for psplash Compiling and installing psplash... Checking dependencies for sysvinit Compiling and installing sysvinit... Entering /opt/DM355SDK840402/toolchain... Build complete Entering arch... Checking dependencies for base Compiling and installing base... Entering mach... Checking dependencies for base Compiling and installing base... Entering proprietary_src... Checking dependencies for dvsdk_2_00_00 Checking dependencies for xdctools_3_10_05 Compiling and installing xdctools_3_10_05... Compiling and installing dvsdk_2_00_00... svn: OPTIONS of 'https://gforge.ti.com/svn/dmai/trunk/davinci_multimedia_application_interface/dmai': could not connect to server (https://gforge.ti.com) make[3]: *** [patched] Error 1 Error building dvsdk_2_00_00 make[2]: *** [dependency_build] Error 1 make[1]: *** [proprietary_src_build] Error 1 make: *** [fs_build] Error 2 kiran@kiran-laptop:/opt/DM355SDK840402$
Dear Friends,
This is regarding the problem I have faced with DM355 board(Leopard board).
I
am trying to create the zImage and rootfile system from the source
provided from ridgerun. But during the make of rootfs compilation ,it
try to take
some package from TI website (https://gforge.ti.com/svn/dmai/trunk/davinci_multimedia_application_interface/dmai). My internet connection is working.
I am not able to access those packages as for accessing that web
link some authentication has required(user id and password). I have
tried through basic registration but cannot able to access.My Internet
connection is perfectly working
I have already installed xdctools_3_10_05 and dvsdk_2_00_00.
Can someone please help me on that? For More information I am attaching the log file of the error.
Regards
Kiran Thakkar