This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

no output of gingerbread on beagle-xm



Hi,

I have gingerbread working on beagleboard-xm now and i have connected one lcd+touch screen through hdmi-hdmi cable as this lcd does'nt have dvi port on it.

I am not able to get any output on this screen. 

I am using this script for making boot.scr;

#!/bin/sh

cat <<EOF > boot.cmd

if fatload mmc 0 80200000 uImage

then

 echo ***** Kernel: /dev/mmcblk0p1/uImage *****

fi

echo ***** RootFS: /dev/mmcblk0p2 *****

setenv bootargs 'console=ttyS2,115200n8 androidboot.console=ttyS2 mem=256M root=/dev/mmcblk0p2 rw rootfstype=ext3 rootdelay=1 init=/init ip=off mpurate=1000 omap_vout.vid1_static_vrfb_alloc=y vram=16M omapfb.vram=0:8M,1:4M,2:4M omapfb.mode=dvi:640x480MR-16 omapdss.def_disp=dvi'

bootm 0x80200000

EOF

mkimage -A arm -O linux -T script -C none -a 0 -e 0 -n 'Execute uImage.bin' -d boot.cmd boot.scr