Other Parts Discussed in Thread: OMAP-L137, AM1707
Hi,
We are currently using EVM OMAPL137 board & DaVinci-PSP-SDK-03.20.00.12 for linux.
For loading dsp-spi-ais, arm ubl-spi & U-boot we are using OMAP-L137_FlashAndBootUtils_2_20.
we have followed the link given below for how to use serial flasher for OMAPL137
http://processors.wiki.ti.com/index.php/Serial_Boot_and_Flash_Loading_Utility_for_OMAP-L137
But after executing the given command sfh_OMAP-L137.exe -flash_dsp <DSP UBL AIS file> <ARM UBL binary file> <binary application file> it gives the following messages
(AIS Parse): BOOTME received!
(AIS Parse): Performing Start-Word Sync...
(AIS Parse): Performing Ping Opcode Sync...
(AIS Parse): Processing command 0: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 14912-Byte section to address 0x80000000.
(AIS Parse): Processing command 1: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 784-Byte section to address 0x80004240.
(AIS Parse): Processing command 2: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 32-Byte section to address 0x80004550.
(AIS Parse): Processing command 3: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 20-Byte section to address 0x80004590.
(AIS Parse): Processing command 4: 0x58535906.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Performing jump and close...
(AIS Parse): AIS complete. Jump to address 0x800034C0.
(AIS Parse): Waiting for DONE...
(AIS Parse): Boot completed successfully.
Waiting for SFT on the OMAP-L137...
The board kind of hangs at above given condition.
Can anyone provide me solution for above given issue.
Thanks & Regards
Jitendra