Hello,
My customer is using the OMAP-L137 in their system. They would like to know if they can AES encrypt 4x VoIP channels (each at 64Kbps) using the ARM9 CPU. Would TI or the community have some benchmarking on this?
I did find a research paper showing a side by side comparison of AES encryption ran on a C6201 and a Pentium-Pro, both running at 200MHz. The throughput was well above 50Mbps for the Rijndeal Algo. In comparison, the four channels VoIP traffic at a total of 256Kbps (4x64Kbps) is well below 1% of what either the C6201 and the Pentium-Pro were able to encrypt/decrypt. I believe it might be safe to assume that the ARM9 at 375MHz-456MHz can do this with lots of headroom but some benchmarking data would be welcome.
Thanks
Electrons4me