This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reference projects for LogicPD AM3517 Starter Kit

Other Parts Discussed in Thread: AM3517

Hello,

I have a Logic PD AM3517 Starter kit and and working with Code Composer Studio.  Can't open Code Composer Studio project file from examples...

I am trying to import or open one of the BSL CCS example project files but CCS does not appear to recognize the .pjt file as a project file.

My version of Code Composer Studio is 
5.0.1.201012231000

Build id: N201012231000

It is running on the recommended version of Ubuntu Linux 10.04.

The project file I am trying to either import or open as pre-existing is

test_menu.pjt

If I manually open test_menu.pjt with a text editor is indeed a CCS project file.

Why doesn't Code Composer Studio open this?

I saw there are some CCS support files in the BSL. One of them mentioned copying a .gel file to a cc folder but the only folder in CCS having .gel files is an emulator folder.

Have not done anything else with the support files yet...

Thanks!

Paul