Other Parts Discussed in Thread: TMS320C6474
Hi, In the design we have interfaced 88E1111 Marvell's ethernet PHY device with TMS320C6474. Upon initialization, the device detects the link (1000Mbps or 100Mbps) and transmit LED is also active. LInk partner (i.e. PC) receive LED is also blinking. However we could not see any data. SGMII w/o clock interface is used to interface 88E1111 with DSP. It seems to be PHY configuration issue. MDIO command interface is working without any issue. Could anybody have the required register settings for 100Mbps and 1000Mbps? 88E1111 has "PHY Specific control registers" whose details are not clear. Thanks.