Hello,
I noticed that DM365 EVM is equipped with the following CPLD and NAND flash.
|
Mfr |
P/N |
Description |
QTY |
Usage |
|
Altera |
EPM2210GF256C5N |
IC,BGA256,FPGA,2210 GATES,MAX II,1.8V |
1 |
CPLD Bank |
|
Micron |
MT29F16G08FAAWC:A |
IC,TSOP48,NAND FLASH,16G,3.3V |
1 |
NAND Flash |
|
Samsung |
KFG1G16U2B-DIB6000 |
IC,BGA63,ONE NAND FLASH MEMORY,1G |
1 |
CPLD Bank Host/EMIF DC Interface |
I wonder what is the usage of these parts and if they are required in a normal design based on DM365/DM368.
Thanks,
Mohammad