Other Parts Discussed in Thread: DM3730
Hi All,
I start to work on a design using DM3730 for SDR purpose.
Just wonder the following two while reading specs and some reference schematics
(1) For memory, the few designs I read uses POP memory, and in common 512MB.
In order to have 1GB addressing space in total, I assume it connects 512MB x 2 chips, using both CS0 & CS1. Am I right?
Or can I do POP memory with 1GB chip?
(2) For SD card or uSD, the matter like SD/SDHC or its class, is it determined by the DM3730, or the way / sw that I read/write to the SD card?
I shall follow the designs to boot to TF/SD, but wanna use a faster 4GB/8GB class 10.
Thank you for answering.
Regards,
Alex