Other Parts Discussed in Thread: OMAP3530
I recently installed CCS Version: 5.1.0.20110512180 and wanted to work with the OMAP3530 IPC Notify project examples. I was able to locate and build the OMAP3530 Notify(DSP) example using the C6000 Project wizard, but there is no equivalent OMAP3530 Notify(ARM) example in the ARM Project wizard.
Is the ARM side of the OMAP3530 IPC Notify example available from another source?