This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Codec Server Integration In Netra

Expert 2030 points

From the reply to this post: http://e2e.ti.com/support/dsp/integra_dsparm/f/625/p/110293/405986.aspx and from the code in openmax test bench (G711 encoder) in EZSDK 5_01_01_80 [ti-ezsdk_dm816x-evm_5_01_01_80/example-applications/omtb_01_00_00_02/packages/ti/sdo/omtb/dm816x/dspC67x/src] , it seems that DSP OpenMAX audio component will be running on c674x DSP in Netra to provide  MP3, AAC audio encoding/decoding. 

DSP Openmax component SYS/BIOS task will have to be configured by DSP codec engine server integrator for priority level, trace level, stack size, so it runs well with other VISA based xDM algorithms (c6accel, IUniversal, Custom Codecs etc.)1 running on the DSP codec engine server.

This to me means DSP codec server integrator's role will have to change. 

When will the user guide2 be updated to provide help for such an integration?

Will there be DSP examples of  Codec server + OpenMAX  in the EzSDK?

 

Regards

RV

1We currently include xDM algorithm in GenServer generated server.cfg file and add different codecs (c6accel, IUniversal, video analytics etc.). Finally we do a xdc build to get DSP Codec Engine server binary. These are then callable from linux client application running on ARM A8.

2 http://processors.wiki.ti.com/index.php/Codec_Engine_Server_Integrator_User's_Guide