Other Parts Discussed in Thread: OMAP3530
I have been trying to get 720Mhz support OMAP3530 A8_1_02 BSP.
I have a OSDESIGN with PMExt and DVFS Constrained Adapter selected. I do not have any Policy Adapters selected.
I modified the "OpmCeiling" registry setting from the default 5 to 6.
The "OpmInit" is still set at default 5.
I noticed I am still getting console messages showing different OPM settings after powerup even thought I am not changing anything.
The final message shows OPM2 and the BSP Information from the control panel shows 250Mhz. (again I DO NOT have any Policy Adapters selected from the catalog).
If I do a "do opm ?" I see Current frequencies: MPU-250.00 ...
If I do a "do opm 6" I see it set to OPM6 but then it pops back to OPM2 right away.
If I do a "do opm ?" again it still shows MPU-250.00
So how do I get 720Mhz support?
How can I manually scale the operating frequency up and down?