Other Parts Discussed in Thread: THS8200, TVP7002
dear all:
I want to use tvp7002 and ths 8200 to make a video format conversion,it's used for DM648EVM since the board can not input a VGA signal and output a VGA signal,so my ideal is one tvp7002 and one ths8200 for input conversion,VGA to YPbPr,and the same devices for the output,YPbPr to VGA.i have read the TVP7002 evm user guide,the I2C configuration is completed via a software named winvcc4,what i want to ask is that can i use the software to success config all these four chips via a parallel port,cause the device have two i2c addresses.there are few information about the software,Glad for your reply,thank you.
wei yang