Hi,
again I am facing problems to run the SD Card Examples on my ezDSP5505 (REV.C). The examples are build without problems, but the detection of the SD Card (2GB Kingston) always fails. I have already changed the csl_general.h and the set MMCSD Channel to CSL_MMCSD1_INST which I have the SD Slot connected to.
MMCSD-ATAFS TESTS!
MMCSD-ATAFS POLL MODE TEST!
No Card detected
Please Insert SD Card
SD card initialization Failed
MMCSD-ATAFS POLL MODE TEST FAILED!!
MMCSD-ATAFS DMA MODE TEST!
No Card detected
Please Insert SD Card
SD card initialization Failed
MMCSD-ATAFS DMA MODE TEST FAILED!!
MMCSD-ATAFS TESTS FAILED!!
I have checked the signals CLK,CMD,DAT0-DAT3 and VCC without having the SD Card inserted and I am sure that it can't be a problem of the connection.
I'm using CSL Release 2.10.00.00 and CCS 4.0.0.16. Can anyboby help me with that?
Thanks in advance,
Moritz