This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6747 CSL Library

Hello,

I am looking for C6747 CSL Library, (with an EDMA3 examples), I dont have it on disk that comes with OMAPL137 EVM, and I cannot find it on site (that's strange, almost every other CSL is exits [:^)]).

There is a link to it in one of the forums here, but it is broken.

Please Help

 

Regards

Arye

 

  • The CSLr is packaged with the PSP drivers which, by default, should be installed in the C:\Program Files\Texas Instruments\pspdrivers_01_xx_xx folder. If the pspdrivers folder does not exist you may need to install it from the SDK located in the C:\C674x_dsp_1_00_00_11 directory. Alternately you can find the PSP installer separately here.