Other Parts Discussed in Thread: OMAP-L138
Hello, In my custom board the Phy is connected to the OMAP-L138 processor through "enable switch", i.e. I can enable disbale the Phy by changing a known GPIO output in the OMAP. I see starnge thing: when I disable the Phy the OMAP, reset itself, as if It cannot work without Phy. I see it not only in u-boot, but also when configuring the OMAP in the CCS with the GEL file. Does the OMAP cannot work without Phy ? Best Regards, Ran