Other Parts Discussed in Thread: OMAP-L137
Hello,
I am trying to upload a simple program I wrote for OMAP L137 into device flash on OMAP-L137 Starter Kit. I follow the sequence described in:
http://wiki.davincidsp.com/index.php/Serial_Boot_and_Flash_Loading_Utility_for_OMAP-L137
The problem occures, when I set the BOOT switches and checking communication with Hypertherminal:
Instead of "BOOTME" prompt I get next sequnce:
U-Boot 1.3.3 (Apr 23 2009 - 17:32:00)
I2C: ready
DRAM: 64 MB
*** Warning - bad CRC, using default environment
In: serial
Out: serial
Err: serial
ARM Clock : 300000000 Hz
More than one PHY detected.
Hit any key to stop autoboot: 0
U-Boot >
and a baudrate is 115200 instead of 230400 as described in the document.
Please help.
Thank You
Arye Lerner