Hi,
I've got myself a beagleboard XM to mess about with , and set the terminal settings are per recommend of : -
A - Serial Device : /dev/ttyS0 |
| B - Lockfile Location : /var/lock |
| C - Callin Program : |
| D - Callout Program : |
| E - Bps/Par/Bits : 115200 8N1 |
| F - Hardware Flow Control : No |
| G - Software Flow Control : No
However, The characters set still appears to be incorrect, as display appears as follows : -
Fi~oerþi~z md5 f1z49z2zeaz36zbcz1bzd9zy1z?1z4cza4z?f:2fzc4z4f
Sai~o Dr.y¢logd/klogdz doneom2.3Mi~icom2.3Mi~icom2>3Mi~icom2>3doþbea>
Sa/,
>-------> ...................j
| | >-.
| | |-----.----->-----.| | >----..----->----->
| | | __ | ---/| /--.| >-/| | |
| | | | | |--- || --/| | | / | | | |
/---/---/--/--/--. |-----//----//--/ /-----/-/-/-/
-/ |
/---/
The A~o>om Di>ib}_þ beaoleboad yS2
A~o>om 2010>?-e¢-20100x20 beaoleboad yS2
beaoleboad logi~z
Can anyone recommend who to fix this, thanks
Brian