Hi there,
I'm working on the bringup of a board that's based on the Beagleboard-XM design. The bringup has been going well and I've been impressed by the overall quality and ease of development with xloader and u-boot. Most things worked straight off the bat so thanks to the TI and other folk who did the hard work for that. I've posted the full patches that I've made to the xloader and u-boot codebase for my bringup here: https://sites.google.com/site/w2debug/debug1 Hopefully, I'll be able to get it merged into upstream with some time.
Ok, so the problem I wanted to talk about has to do with GPMC. On this board, I used GPMC cs4 to interface with a SMSC 9220 ethernet controller. This is much the same as what is done on other similar boards such as the TI EVM. When I tested this, I found that in u-boot, I'm able to detect and read registers from the SMSC9220 like the ID register and BYTE_TEST register. But it fails to establish link state, and fails to send out any packets. When I debugged this further, I found that it appears that GPMC writes to the SMSC9220 controller weren't having any effect. For example, writing various patterns to the INT_EN register always read back as 0. Same is true with PMT_CTL. My consolelog that shows this is appended below. I have setup GPMC cs4 in what I believe is the correct way:
+static u32 gpmc_net_config[GPMC_MAX_REG] = {
+ NET_GPMC_CONFIG1,
+ NET_GPMC_CONFIG2,
+ NET_GPMC_CONFIG3,
+ NET_GPMC_CONFIG4,
+ NET_GPMC_CONFIG5,
+ NET_GPMC_CONFIG6,
+ 0
+};
+ /* Configure GPMC registers */
+ enable_gpmc_cs_config(gpmc_net_config, &gpmc_cfg->cs[4],
+ CONFIG_SMC911X_BASE, GPMC_SIZE_16M);
+
+ /* Enable off mode for NWE in PADCONF_GPMC_NWE register */
+ writew(readw(&ctrl_base ->gpmc_nwe) | 0x0E00, &ctrl_base->gpmc_nwe);
+ /* Enable off mode for NOE in PADCONF_GPMC_NADV_ALE register */
+ writew(readw(&ctrl_base->gpmc_noe) | 0x0E00, &ctrl_base->gpmc_noe);
+ /* Enable off mode for ALE in PADCONF_GPMC_NADV_ALE register */
+ writew(readw(&ctrl_base->gpmc_nadv_ale) | 0x0E00,
+ &ctrl_base->gpmc_nadv_ale);
My pinmux looks correct and I verified that the chip select works, as can be seen since register reads work fine. So I'm a bit confused why writes wouldn't work. I would welcome any advice or suggestions on what I should check out.
U-Boot 2011.06-rc1-00063-gb3a6f32-dirty (Jun 05 2011 - 19:51:24)
OMAP3630/3730-GP ES2.1, CPU-OPP2, L3-165MHz, Max CPU Clock 1 Ghz
OMAP3 Wiser2 board + LPDDR/NAND
I2C: ready
DRAM: 256 MiB
NAND: 256 MiB
MMC: OMAP SD/MMC: 0
*** Warning - bad CRC, using default environment
In: serial
Out: serial
Err: serial
Wiser2
Die ID #420800029ff800000160a74507005015
Net: smc911x: test register writes to INT_EN, initial value=0x0
smc911x: wrote 0xffffffff, read value=0x0
smc911x: WARNING: WRITE mismatch wrote 0xffffffff, read value=0x0
smc911x: wrote 0x5555aaaa, read value=0x0
smc911x: WARNING: WRITE mismatch wrote 0x5555aaaa, read value=0x0
smc911x: wrote 0xc001f00d, read value=0x0
smc911x: WARNING: WRITE mismatch wrote 0xc001f00d, read value=0x0
smc911x: wrote 0x0, read value=0x0
smc911x-0
Hit any key to stop autoboot: 0
OMAP3 beagleboard.org # setenv ethaddr 00:22:33:44:55:66
OMAP3 beagleboard.org # bootp
smc911x: detected LAN9220 controller
smc911x: autonegotiation timed out
smc911x: MAC 00:22:33:44:55:66
BOOTP broadcast 1
Thanks,
jayakumar