This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

3 video inputs on DaVinci?



I'm using the DM6467T, which can support only two SD video input channels.  I was speaking to a vendor tech support about something else.  He said you could get 3 SD video input channels into a DaVinci chip. Then he said dual core.  Then he said OMAP.  

Being far from familiar with the TI product line, I'm wondering if I need to change processors.  I do need the DSP for heavy-duty video analytics processing.  Is there some other chip that includes the DSP, plus can do 3 SD video inputs?

Thanks,

Helmut