Greetings,
I apologize in advance if this is a dumb question or it has been answered already in sort of FAQs.
I am just wondering if anyone could kindly clue me regarding how to handle SmartReflex issue when I have several DSP devices, such as TCI6488, on board. Do I need to have separate adjustable power regulator (such as PTH08T240F) for each TCI6488 device or a single common one could be used to supply the core voltage to all TCI6488 (though this seems infeasible to me)?
In case that I am doing the ATCA DSP blade and plan to accomodate 20x TCI6488, it looks a little bit tough to host 20x power regulators for each individual TIC6488 device. I was thinking that only DSP devices reside near hot spot area (in terms of temperature) deserving such flexibility for dynamic power management.
Any comment or tip would be highly appreciate!
David