Other Parts Discussed in Thread: CCSTUDIO
hi,
I found several reply about this matter. Now I know this is xdcpath problem.
Although I have tried to solve this matter with several ways, I still don't know why.
Anyone help me to solve this problem.please
------------ dm648_evm_vport_st_sd_compositor_sample.pjt - Debug ------------
[dm648_evm_vport_st_sd_compositor_sample.cfg] "C:\xdc_2_95_02\xs.exe" xdc.tools.configuro.ccs --xdcpathsfile="xdcpaths.dat" -pti.platforms.evmDM648 -rdebug -w --tcf -t ti.targets.C64P -c "C:/CCStudio_v3.3/C6000/cgtools" --bios "C:/CCStudio_v3.3/bios_5_33_06" -o "xdcconfig" dm648_evm_vport_st_sd_compositor_sample.cfg
Info: running XDC configuration using package path:
C:\edma3_lld_1_05_00\packages
Z:\pspdrivers\pspdrivers_\packages
C:\CCStudio_v3.3\bios_5_33_06\packages
C:\xdc_2_95_02\packages
The configuration step is now running:
making package.mak (because of package.bld) ...
generating interfaces for package xdcconfig (because package/package.xdc.xml is older than package.xdc) ...
configuring dm648_evm_vport_st_sd_compositor_sample.x64P from package/cfg/dm648_evm_vport_st_sd_compositor_sample_x64P.cfg ...
js: "C:/xdc_2_95_02/include/utils.tci", line 488: exception from uncaught JavaScript throw: Error: Can't find import file: 'ti/sdo/pspdrivers/system/dm648/bios/evmDM648/i2c/dm648_i2c0.tci' (not found along 'C:\dvsdk_1_11_00_00_DM648\pspdrivers_1_10_00\packages\ti\sdo\pspdrivers\system\dm648\bios\evmDM648\video\sample\build\sd_compositor/;.;C:/edma3_lld_1_05_00/packages;Z:/pspdrivers/pspdrivers_/packages;C:/CCStudio_v3.3/bios_5_33_06/packages;C:/xdc_2_95_02/packages;C:/dvsdk_1_11_00_00_DM648/pspdrivers_1_10_00/packages/ti/sdo/pspdrivers/system/dm648/bios/evmDM648/video/sample/build/sd_compositor;C:/xdc_2_95_02/packages;..;C:/xdc_2_95_02;C:/xdc_2_95_02/etc;C:/CCStudio_v3.3/bios_5_33_06/packages/ti/bios/include;c:\xdc_2_95_02/include;c:\xdc_2_95_02/packages')
"C:/dvsdk_1_11_00_00_DM648/pspdrivers_1_10_00/packages/ti/sdo/pspdrivers/system/dm648/bios/evmDM648/video/sample/build/sd_compositor/dm648_evm_vport_st_sd_compositor_sample.tcf", line 26
"C:/xdc_2_95_02/include/utils.tci", line 566
"C:/xdc_2_95_02/include/utils.tci", line 484
"./dm648_evm_vport_st_sd_compositor_sample.tcf", line 2
"C:/xdc_2_95_02/include/utils.tci", line 566
"C:/xdc_2_95_02/include/utils.tci", line 484
"./package/cfg/dm648_evm_vport_st_sd_compositor_sample_x64P.cfg", line 634
"./package/cfg/dm648_evm_vport_st_sd_compositor_sample_x64P.cfg", line 605
"C:/xdc_2_95_02/packages/xdc/cfg/Main.xs", line 182
"C:/xdc_2_95_02/packages/xdc/cfg/Main.xs", line 151
"C:/xdc_2_95_02/packages/xdc/xs.js", line 137
gmake.exe: *** [package/cfg/dm648_evm_vport_st_sd_compositor_sample_x64P.c] Error 1
*************************
Configuration step failed.
*************************
Explanation:
-----------
XDC tools could not find file 'ti/sdo/pspdrivers/system/dm648/bios/evmDM648/i2c/dm648_i2c0.tci' in your package path.
If this is a valid script name --
To correct this error, you must locate a directory on your system
that contains that script and add it to your package path.
(You can use an absolute path or one relative to your project,
e.g. '../../myTconfScripts/'.)
If you are unsure which script attempted to load the missing script,
please look at the list of scripts located below the original error line above.\n
Please review the above information carefully to correct this configuration error.
[psp_bios_vport_byte_swap.c] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -g -q -@"=C:/dvsdk_1_11_00_00_DM648/pspdrivers_1_10_00/packages/ti/sdo/pspdrivers/system/dm648/bios/evmDM648/video/sample/build/sd_compositor/xdcconfig/compiler.opt" -fr"./Debug" -i"C:/dvsdk_1_11_00_00_DM648/pspdrivers_1_10_00/packages" -d"_DEBUG" -d"CHIP_DM648" -mv6400+ -mv64+ -@"../build/sd_compositor/Debug.lkf" "psp_bios_vport_byte_swap.c"
[psp_bios_vport_sd_compositor.c] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -g -q -@"=C:/dvsdk_1_11_00_00_DM648/pspdrivers_1_10_00/packages/ti/sdo/pspdrivers/system/dm648/bios/evmDM648/video/sample/build/sd_compositor/xdcconfig/compiler.opt" -fr"./Debug" -i"C:/dvsdk_1_11_00_00_DM648/pspdrivers_1_10_00/packages" -d"_DEBUG" -d"CHIP_DM648" -mv6400+ -mv64+ -@"../build/sd_compositor/Debug.lkf" "psp_bios_vport_sd_compositor.c"
"C:/dvsdk_1_11_00_00_DM648/pspdrivers_1_10_00/packages/ti/sdo/pspdrivers/drivers/vport/vportdis.h", line 45: fatal error: could not open source file "ti/sdo/edma3/drv/edma3_drv.h"
1 fatal error detected in the compilation of "psp_bios_vport_sd_compositor.c".
Compilation terminated.
>> Compilation failure
[psp_bios_vport_st_sample_main.c] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -g -q -@"=C:/dvsdk_1_11_00_00_DM648/pspdrivers_1_10_00/packages/ti/sdo/pspdrivers/system/dm648/bios/evmDM648/video/sample/build/sd_compositor/xdcconfig/compiler.opt" -fr"./Debug" -i"C:/dvsdk_1_11_00_00_DM648/pspdrivers_1_10_00/packages" -d"_DEBUG" -d"CHIP_DM648" -mv6400+ -mv64+ -@"../build/sd_compositor/Debug.lkf" "psp_bios_vport_st_sample_main.c"
Build Complete,
2 Errors, 0 Warnings, 11 Remarks.