Hi,
Can anyone point me in the direction of a U-Boot image for the L138 EVM that includes support for the MMC/SD card. The one I downloaded from the LogicPD site does not appear to support this.
Cheers,
John.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can anyone point me in the direction of a U-Boot image for the L138 EVM that includes support for the MMC/SD card. The one I downloaded from the LogicPD site does not appear to support this.
Cheers,
John.
The pre-built images at TI's Arago Project might have SD support. Main site:
http://www.arago-project.org
The site appears to have only one, older, release for the L138.
http://arago-project.org/files/releases/2009.11/images/da850-omapl138-evm/
I think the latest DVSDK has pre-built binaries for the L138 but it's a really big package to download.
A quick look inside the platform support package (the PSP, version 03.20.00.14) included with DVSDK 4.01 (latest is 4.02 I believe) shows that the u-boot config header has support for mmc:
#define CONFIG_MMC
#define CONFIG_GENERIC_MMC
#define CONFIG_DAVINCI_MMC
#define CONFIG_MMC_MBLOCK
Regards, Daniel
Thanks for your responses.
Yes: the image in PSP 03.20.00.14 did have support for MMC.
Thanks again.