hi
i am working with dvsdk on beagleboard-xm which runs with dm3730 processor
i have used dvsdk_dm3730-evm_4_01_00_06_setuplinux to install the dvdsk on host..the build was clean. but the codec engine is not working
below is the occurred errors when i try to execute the decode demo...
root@beagleboard-dvsdk:/usr/share/ti/dvsdk-demos# ./decode -v ../data/
videos/davincieffect.mpeg4
Decode demo started.
[ 251.764312] Start address is covered by existing entry, can not
create TLB entry for address: [0x85900000] size: [0x100000]
[ 251.775634] DSP_init status [0x80008050]
Error: Failed to open codec engi[ 251.782623] Start address is
covered by existing entry, can not create TLB entry for address:
[0x85900000] size: [0x100000]
ne decode
[ 251.795410] DSP_init status [0x80008050]
Error: Failed to open codec engine decode
lsmod output...
root@beagleboard-dvsdk:/home/dsp# lsmod
Module Size Used by
sdmak 3719 0
lpm_omap3530 6537 0
dsplinkk 124358 1 lpm_omap3530
cmemk 21318 0
omaplfb 8770 0
bufferclass_ti 4838 0
pvrsrvkm 129642 2 omaplfb,bufferclass_ti
any idea what could be went wrong??