This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C66x EMAC IEEE1588 support



Tell me please if there is a representatiive description of TMS320C66x EMAC IEEE1588 time synchronization module?

  • Igor,

    You can find details related to the IEEE 1588 time synchronization module in section 2.3.5 of the Keystone Gigabit Ethernet Switch Subsystem User Guide (http://www.ti.com/litv/pdf/sprugv9). 

    Regards,

    Derek

     

  • I'm sorry but this section contains only a bit more than nothing and gives no presentation of how this module operates and particularly of its architecture (despite of the caption of the section). There is a definition of registers of the module in this user guide but it explains not very much. For example, the meaning of RFTCLK_SEL field is given there as device specific but device specific data sheets gives no information on RFTCLK_SEL and of the time synchronization module in general. Maybe some other more mature TI DSP has the same module described in detail?

  • Igor,

    Let me look into this some more and see what I can find. I will get back with you soon.

    Regards,

    Derek

  • Thank you, I hope the matter will be clarified finally

  • Igor,

    The IEEE 1588 rtfclk_sel should be shown in the data manuals. As you stated, this information is currently missing, so thank you for brining it to our attention. We are currently working to add this information to the data manuals. I am not sure when the updated data manual will be released, I am providing the information about the RTFCLK_SEL register now so that you can have the details immediately.

    To select the desired clock, program RTFCLK_SEL[2:0] in the Time Synchronization submodule in the Ethernet switch. The bit values of this register correspond to the following clocks:

    C6670

    000 sysclk2

    001 sysclk3

    010 timi0

    011 timi1

    100 reserved

    101 reserved

    110 reserved

    111 reserved

     

    C6678

    000 sysclk2

    001 sysclk3

    010 timi0

    011 timi1

    100 tsip0 clka

    101 tsip0 clkb

    110 tsip1 clka

    111 tsip1 clkb

    I am still working on getting more details for you about the IEEE 1588 module.  I will provide these details as they are available, and will also make sure that they get included in the user guide.

    Regards,

    Derek

  • Igor, 

    The GbE switch user guide has been updated to provide more information about the time synchronization module. It will be available for download in the near future. The document with the updates will be marked as revision A.

    Regards,

    Derek