Other Parts Discussed in Thread: AM3517
Hello,
I’m looking to update a Logic PD AM3517 SOM from a 2.6.31-rc7 kernel to the last v2.6.37_OMAPPSP_04.02.00.07 tagged kernel.
Using the 2.6.37 kernel ,I get problems with the UBIFS partitions. After formatting and rebooting, ubiattach gives following errors
UBI: attaching mtd5 to ubi0
UBI: physical eraseblock size: 131072 bytes (128 KiB)
UBI: logical eraseblock size: 129024 bytes
UBI: smallest flash I/O unit: 2048
UBI: sub-page size: 512
UBI: VID header offset: 512 (aligned 512)
UBI: data offset: 2048
UNCORRECTED_ERROR default
UNCORRECTED_ERROR default
UBI error: ubi_io_read: error -74 (ECC error) while reading 64 bytes from PEB 1:0, read 64 bytes
UNCORRECTED_ERROR default
…
All the MTD Test tools successes, except the sub-page one:
mtd_subpagetest: MTD device: 6
mtd_subpagetest: MTD device size 268435456, eraseblock size 131072, page size
2048, subpage size 512, count of eraseblocks 0, pages per eraseblock 0, OOB
size 64
mtd_subpagetest: scanning for bad eraseblocks
…
mtd_subpagetest: scanned 2048 eraseblocks, 4 are bad
mtd_subpagetest: erasing whole device
mtd_subpagetest: erased 2048 eraseblocks
mtd_subpagetest: writing whole device
mtd_subpagetest: written up to eraseblock 0
mtd_subpagetest: written up to eraseblock 256
…
mtd_subpagetest: written up to eraseblock 1792
mtd_subpagetest: written 2048 eraseblocks
mtd_subpagetest: verifying all eraseblocks
mtd_subpagetest: error: read failed at 0x0
mtd_subpagetest: error -74 occurred
I made a test with the last TI official BSP, based on a 2.6.32 kernel. This problem doesn’t exist, but I had to ubiformat the partition without sub-pages …. ?
Any idea about what’s going on ? What is the state of the omap nand driver ? Something I missed for this update ?
Cheers
David