Could someone please verify the size of the transmit and receive buffers on the C6a816x EVM module (the older DDR2 revision). All datasheet references suggest a 5kB buffer for both Tx and Rx but then on page 1124 of the TRM there is the following note:
Note: SC_McBSPOCP10GS60 implements 512B (128 x 32 bits memory) transmit and receive buffer,
while SC_McBSPOCP20GS60 implements 5 kB (1280 x 32 bits memory) transmit and 5KB receive
buffer (AUDIOBUFFER support).
The port behavior I am seeing seems to suggest that the receive buffer may in fact only be 512 bytes? Is this true?