Hi,
I am working on TCI6486 based board. I am able to successfully execute the helloworld.pjt and cfgdemo.pjt projects in TCI6486 NSP using NDK ver 2.0.0.
But I am get the following failed message when I execute the client.pjt project of the NSP:
TCP/IP Stack Example Client
MAC Address read from EFUSE: 08-00-28-04-E4-5E
Core Number on which NDK is running = 0
EMAC has been started successfully
Registeration of the EMAC Successful
Service Status: DHCPC : Failed : : 000
Service Status: Telnet : Failed : : 000
Service Status: HTTP : Failed : : 000
Can anybody help me on this...
Thanks,
Amitkumar Solanki
(amitkumar.solanki@einfochips.com)