Other Parts Discussed in Thread: SYSCONFIG
I have a problem with my board that mounts an OMAP3530DCUS with a 512Mb LPDDR Micron x32 with this pn. MT46H16M32LFCM-6:B (datasheet link http://www.micron.com//products/ProductDetails.html?product=products/dram/mobile_lpdram/MT46H16M32LFCM-6).
I state that the same board with a mounted LPDDR 1Gb (Micron pn. MT46H32M32LFCM-5:A) works correctly. So the connection I think it is right.
I have modified the register initialization in function sdrc_init in the file board-beagle.c of BAREBOX but after the download of it the board dosn't give me any signal of life or activity (no prompt and no echo with terminal).
I list the init function I'm using...
static void sdrc_init(void)
{
/* SDRAM software reset */
/* No idle ack and RESET enable */
writel(0x12, SDRC_REG(SYSCONFIG));
sdelay(100);
/* No idle ack and RESET disable */
writel(0x10, SDRC_REG(SYSCONFIG));
/* SDRC Sharing register */
/* 32-bit SDRAM on data lane [31:0] - CS0 */
/* pin tri-stated = 1 */
writel(0x00000100, SDRC_REG(SHARING));
/* ----- SDRC Registers Configuration --------- */
/* SDRC_MCFG0 register */
writel(0x02482099, SDRC_REG(MCFG_0));
/* SDRC_RFR_CTRL0 register */
writel(0x4e201, SDRC_REG(RFR_CTRL_0));
/* SDRC_ACTIM_CTRLA0 register */
writel(0x8a9dB4C6, SDRC_REG(ACTIM_CTRLA_0));
/* SDRC_ACTIM_CTRLB0 register */
writel(0x21114, SDRC_REG(ACTIM_CTRLB_0));
/* Disble Power Down of CKE due to 1 CKE on combo part */
writel(0x00000081, SDRC_REG(POWER));
/* SDRC_MANUAL command register */
/* NOP command */
writel(0x00000000, SDRC_REG(MANUAL_0));
/* Precharge command */
writel(0x00000001, SDRC_REG(MANUAL_0));
/* Auto-refresh command */
writel(0x00000002, SDRC_REG(MANUAL_0));
/* Auto-refresh command */
writel(0x00000002, SDRC_REG(MANUAL_0));
/* SDRC MR0 register Burst length=4 */
writel(0x00000032, SDRC_REG(MR_0));
/* SDRC DLLA control register */
writel(0x0000000A, SDRC_REG(DLLA_CTRL));
return;
}
What could be the problem?
Please help me. I'm quite desperated.
Thanks very much,
Daniele Licini.