This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WINCE Debug Build Error



Hi,

I have the same issue on BSP_WINCE_ARM_A8_01_02_00 as that referenced in

http://e2e.ti.com/support/embedded/f/353/t/65534.aspx

 

the debug configuration won't compile and return the same error in the same file, the release configuration compile without errors.

 

I've just installed a new XP SP3 + VS2005, with all updates (VS2005 SP1,...), Windows Platform builder SP1, Windows CE R3 with all QFEs up to april 2011.

I'm trying to compile the latest BSP from texas: BSP_WINCE_ARM_A8_01_02_00_Source

 

Do you have any ideas where the problem could be?

 

thanks

-------------------------------------------------------------

Update:

I've added Network Utilities, Cab File Installer/Uninstaller, and OS Dependencies for .NET Compact Framwork 2.0 to the BSP and now debug config compiles without errors.