This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux Boot L138 EVM

Hello,

I am attempting to boot Linux from an SD card on a L138 EVM. I used the Narcissus tool to create a kernal image and file system and put these onto FAT and ext2 partitions on the SD card respectively. The Linux kernal begins booting and gets a good way through before stalling here:

VFS: Mounted root (ext2 filesystem) on device 179:2.

devtmpfs: mounted

Freeing init memory: 280K

request_module: runaway loop modprobe binfmt-0000

request_module: runaway loop modprobe binfmt-0000

request_module: runaway loop modprobe binfmt-0000

request_module: runaway loop modprobe binfmt-0000

request_module: runaway loop modprobe binfmt-0000

After a couple of minutes the kernal crashes.

Anyone have any idea what I have done wrong?

Cheers,

John.