Other Parts Discussed in Thread: OMAP-L138, OMAPL138
Hello. Is there a DSPBios driver available for the AIC3254 CODEC? Specifically, for the OMAP-L138 (C6747)? If not, what supported CODEC driver would be a good candidate to model after?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The Audio codec is a board specific stuff, and for OMAPL138 EVM we have only provided BIOS PSP Driver(pspdrivers_01_30_01) for AIC3106 CODEC. But for AIC3254 CODEC, you will probably have to write your own driver. You can also refer the AIC3106 CODEC and if it is similar, you can take its reference and design it in the same line.
If the AIC3106 CODEC is available on your board, well you can go ahead with it!.
Thanks & regards,
Raghavendra