This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Hello world program of DSP/BIOS

Hello

I am new to DM6437. After running the DSP/BIOS basic hello world example on CCSv3.3 i want to see the output which i am not able to see.

Please help

 

Vishrav

  • Hi Vishrav,

    What DSP/BIOS version are you using?

    Todd

  • Hi

    I am using bios_5_31_02 version.

    One more thing how to change the number of tasks running parallel in tsk example.

     

    Thanks

    Vishrav

  • Hi Vishrav,

    If you are creating the Basic Example: Hello World example, the printf should come out on the console.

    If you are creating the DSP/BIOS v5.xx Example: Hello example, the Log_printf goes into an internal buffer. You can view the log data via the Tools->RTA->Raw Logs tool. The Log_printf is a smaller footprint and has better performance than printf.

    Regarding the multiple tasks, the TSK are statically created in the tsk.tcf file. You can modify this file via a text editor or via the DSP/BIOS Configuration Tool (right-click on the tsk.tcf file and it gives you both options). Statically creating the TSK helps keep the footprint small. Another option is to simply create the TSK dynamically (e.g. call TSK_create in main()).

    Todd