Other Parts Discussed in Thread: AM1808
Is the Device Identification Register a unique ID for each piece of silicon?
Can this be used as "key" for encryption?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: AM1808
Is the Device Identification Register a unique ID for each piece of silicon?
Can this be used as "key" for encryption?
Thanks
Jamie,
Can be more specific about the register to which you are referring? Are you talking about the DIEID registers in the SYSCFG module, or something else?
As far as I know, there are no registers providing a random or psuedo-random value that would suitable as a cryptographic key or for deriving such a key.
Regards, Daniel
Are the values in these registers (DIEID in SYSCFG) unique to each individual Silicon?
Or is it possible the two parts could have the same DIEID ?
Thanks
E
Eric,
The content of the four DIEID registers, when taken as a 128-bit value, is unique to each piece of silicon. The contents of those registers is not documented and will not be documented. Also, I want to reemphasize that the value should in no way be used for any cryptographic purpose, as it is not random.
In case you are interested, TI did just announce secure versions of these parts that provide protection of IP and code in the system flash. See here for info.
Regards, Daniel
Sorry, you are correct. I guess I forgot which device we were talking about.
I apologize for the confusion.
Regards, Daniel