I am using the LogicPD AM3517 Experimenter board - trying to connect to it's Ethernet port from CCSv5 (Version: 5.0.1.201012231000) on Ubuntu Linux 10.04.
I installed Remote System Explorer in CCSv5 but no dialog came up regarding security file like the example.
Can connect to AM3517 Experimenter serial port and log on @ 115k.
Can ping to AM3517 Experimenter Ethernet Port
I am using the version of Linux installed and shipped on the LogicPD AM3517 Experimenter board. Is it possible that this version does not have ssh or other utilities installed?
The error reported is "Connected Refused" when RSE is used or ssh is used in a shell terminal.