This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SECOND REQUEST: OMAP3530 Notify(ARM) example missing in CCS5.1

 recently installed CCS  Version: 5.1.0.20110512180 and wanted to work with the OMAP3530 IPC Notify project examples.  I was able to locate and build the OMAP3530 Notify(DSP) example using the C6000 Project wizard, but there is no equivalent OMAP3530 Notify(ARM) example in the ARM Project wizard.

Is the ARM side of the OMAP3530 IPC Notify example available from another source?

 

NOTE: I originally posted this response in the Code Composer  Studio Forum and it was moved by TI to this forum.  No further response has been received.