Hai,
We have designed AM3356 based OEM board with 2 Giga Bit DDR3 SDRAM (IS43TR16128C), which has a base speed of 1333. It is working with no issues. Now we need to upgrade the RAM size to 8 Giga Bit. So we choose IS43TR16512B as our chip. But the base speed mentioned is 1600.
Does AM3356 support this DDR3 SDRAM(IS43TR16512B) which has a slightly higher base speed..?
Regards,
Jibin K Mathai