Other Parts Discussed in Thread: CCSTUDIO
Hi,
I have problems when compiling dsk_app in release mode.Here is the log:
[dsk_app.c] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -o3 -fr"C:/CCStudio_v3.3/boards/dsk6455_v2/examples/dsk_app/Release" -mv6400 -@"Release.lkf" "dsk_app.c"
"dsk_app.c", line 109: fatal error: could not open source file "dsk6455.h"
1 fatal error detected in the compilation of "dsk_app.c".
Compilation terminated.
>> Compilation failure
[dsk_appcfg.s62] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -o3 -fr"C:/CCStudio_v3.3/boards/dsk6455_v2/examples/dsk_app/Release" -mv6400 -@"Release.lkf" "dsk_appcfg.s62"
"dsk_appcfg.s62", ERROR! at line 365: [ ***** USER ERROR ***** - ]
Project build options do not match Global configuration settings.
Compiler options do not specify -mv64+, but configuration is for
C64x+
.emsg "Project build options do not match Global configuration settings. Compiler options do not specify -mv64+, but configuration is for C64x+"
"dsk_appcfg.s62", ERROR! at EOF: [E0300] The following symbols are undefined:
2 Assembly Errors, No Assembly Warnings
HWI_INTRMULTLOW
HWI_INTRMULTHIGH
GBL_L2MARMASK1
GBL_L2MARMASK2
GBL_L2MARMASK3
GBL_L2MARMASK4
GBL_L2MARMASK5
GBL_L2CONFIGALLOC
GBL_L2ALLOC
GBL_C641XL2PRIORITY
Errors in Source - Assembler Aborted
>> Compilation failure
Build Complete,
3 Errors, 0 Warnings, 0 Remarks.
I didn't change anything in this example, what should I do fix these errors?
Thanks,
Pete.